The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
igus新基座轴承,用于太阳能支架方轨上的免润滑解决方案07/04/2017
运动塑料专家igus开发出了非常坚固耐磨的igubal基座轴承,用于支撑110毫米的大型方轨。比如,可运用在太阳能电厂的追踪式面板支架上,且无需润滑和维护。在igus内部测试中,轴承的使用寿命已超过70年,且未出现任何问题。 相比前一年,去年可再生能源在电力行业的份额增加超过16%。对于太阳能产业,这意味着需要越来越多具有自动化、免维护跟踪系统的现代太阳能电厂。运动塑料专家igus开发出的igubal基座轴承ESQM-110,可免润滑支撑110毫米的方轴,非常适合上述应用需求。基座由坚固的igumid G材料制成,内球面轴承以耐磨的iglidur J4材料制成,分为上下两部分,易于装配和拆卸。这种解决方案虽然重量轻,但适用于支撑非常高的负载。 在igus实验室中成功模拟测试 igus igubal产品经理Thomas Preißner表示:“为了高度模拟基座轴承的真实使用寿命,我们在轴承上以1.5吨的负载进行连续的摆动测试。正常情况下,太阳能系统每天只摆动一次。而我们的测试每分钟摆动一次,模拟了72年的运转时间。测试完成后,轴承上没有明显的磨损痕迹。” 由于采用球面滑动轴承,可以补偿大型的太阳能电厂方轴上的安装误差。除了太阳能产业,igubal基座轴承也可用于许多其他应用,如X光机或清洗系统。为了给各领域的客户提供高度的设计自由,igus还提供了定制服务,可根据客户要求的方形尺寸定制并在1周内交付。 |