The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
igus 现货供应用于起重机设备供能系统的中压电缆25/04/2017
在起重机和物料输送行业,设备变得越来越大,并且需要全天候地更高动态地运行。这意味着设备对能源的需求和所用部件的要求都越来越高,以保证其一年365天所要承受的不断加大的运行压力。针对这类项目,运动塑料专家igus开发出了chainflex高柔性电缆CFCRANE.PUR系列,来配合低磨损、低噪音的轮式拖链使用。这个系列特别适合长达1000米的超长行程。新款中压电缆CFCRANE.PUR可承受6/10 kV的电压,且因其具有特殊的导体结构和护套材料,可在室内和室外应用。其直径也比常规动力电缆小了20%。 36个月质保承诺的特种电缆现货供应 新款电缆系列适用于弯曲半径10xd的拖链系统。其耐用性已经在igus实验室里获得了证实。和1244种现货供应的igus chainflex高柔性电缆一样,新系列也可获得36个月质保承诺。igus chainflex高柔性电缆部门主管Rainer Rössel表示:“如果客户急需新电缆来替换现有的,也无需等待很久。因为客户可以直接从我们的库存中订购新电缆,并可在最短时间内收到货。”这一快速交付服务同样适用于特殊项目,igus会通过其项目工程团队帮助客户实施。例如,散货装卸或近海领域如果需要装配新的供能系统,igus专家可以从规划阶段开始就提供协助。igus不仅为客户提供拖链和电缆的一站式生产、配送,也提供安全、即插即用的解决方案,非常值得信赖。 |