法兰克福车展:igus微型拖链助力新车安全供能15/09/2017

据福尔萨调查,三分之一的车主在工作日用车超过一小时。趋势表明,因为日益增长的汽车需求,这个用车时间还将在未来几年内持续增长。同时,车主对车内设备的要求也将不断提高。这样一来,汽车势必会日益智能化和电子化, 包括车窗升降器、雨刷、后挡板、转向灯,乃至座椅系统、滑动门、中心控制系统、显示器和扬声器等。无人驾驶和电动交通等未来趋势也需要越来越多的电缆和安全、轻便的供能系统。 共享汽车给电子系统带来新的压力 如今,汽车上的电子系统正面临着新的压力。共享汽车的概念在全球越来越普及。例如,每次出行之前,车门必须通过芯片自动打开。因此,自动门系统的需求从200,000次开关循环增加到了500,000次。共享汽车还会增加每天调节座椅和后视镜的次数,这也给供能系统带来了压力。因此,在狭小空间内对运动电缆进行长期可靠的运行保护是必要的。而igus拖链正是最佳选择。它们即使在极端温度下也可以安全保护和引导电缆。igus拖链以高性能塑料制成,不仅耐腐蚀、免润滑,还十分轻巧。此外,igus拖链的耐磨性成功通过了亚利桑那摩擦测试,同时部件的耐脏污性也符合标准。 E2微型拖链:用于运动和持续供能系统的解决方案 igus将在法兰克福国际车展4号展厅的E23展台展示E2微型拖链等产品。E2微型拖链是专为狭小安装空间设计的,并且已应用在电子滑动门上。现已推出不同尺寸,以便适用于从雨刷到后挡板等各种汽车应用场景,是安全保护能源和信号供应线的理想选择。它的最小尺寸是4.5毫米,是世界上最小的塑料拖链,适用于最狭小的空间。用高性能igumid G材料制成的E2C.10和E2C.15系列拖链能够承受-40°到+80°的温度范围,而且可以实现高达3m/s²的加速度。E2微型拖链的小节距能够确保安静运行,链节之间的大孔销连接则可以保证其拥有更长的使用寿命。因为重量轻,它们特别适合于高动态应用。


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH