Press

Do you have any questions? Need material?
Current press information and ready to publish photo material is available for download here.
We would also be delighted about your call, e-mail or fax!
 
Press contactWould you like to be added to our media distribution list?

Press releases by area

精准且快速移动的igus免润滑转角轴承23/11/2017

在物料搬运和包装行业中,温和且快速的货物运输是极其重要的。更重要的是,产能的提高可以不断推动工厂的速度提升。为此,igus开发出了由高性能塑料iglidur H1制成的用于传动带挠度的转角轴承,特别适用于高速传输应用。现在,该转角轴承系列的原材料已扩展到四种。这些新型的滚轴特点是,在更高的传输速度下其性能表现更好,即使在高温下运行,其使用寿命也很长。此外,在滚轴需要接触腐蚀性清洁剂的工况中,由耐化学性的iglidur H1材料制成的igus转角轴承就是最佳选择。因此,滚轴特别适用于包装、材料输送、自动化和食品技术领域。 多种免润滑转角轴承材料可供选择 为了让传送带实现精确偏转,igus为多种应用领域研发了相应的标准产品材料。除了适用于高速传输的新型材料iglidur H1,还有通用材料iglidur P210,以及符合FDA标准的适用于温度高达90℃工况的iglidur A180和适用于温度高达180℃工况的iglidur A350,这两款材料尤其适用于食品行业。虽然原材料性能不同,但是所有材料制成的滚轴都具有设计紧凑和使用寿命长的特点,能够确保机器的高效运转。


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH