igus微型拖链在极狭小空间内安全引导电缆15/03/2018

从一般的机械工程到医疗技术领域,许多机械部件都被要求节省空间、坚固且易装配。 为了满足这些要求,igus推出了微型拖链E2.10,其内高仅为10毫米且具有最小弯曲半径,特别适合用于狭小的安装空间。此系列拖链的链节仅由底部/侧面部件和横杆组成,并且具有静音运行和电缆保护设计,可以用打开工具实现简便装配。 在机器中的狭小空间内,电缆在高动态运行下安全供能是至关重要的。为了确保这一点,运动塑料专家igus在其产品系列中引入了紧凑的微型拖链。 E2.1拖链系列中的E2.10型号的内高仅为10毫米,外高为15毫米。因此,它非常适合用于极狭小的空间。与E2.1拖链系列的所有链节一样,E2.10拖链的链节也仅由底部/侧面部件和横杆组成,并且可以用螺丝刀从上部两侧轻松打开。 用于快速打开拖链的工具随首次订单一起交付。使用快速打开工具,仅需几秒就能打开拖链,在电缆安装完成后,用手就可以轻松将拖链闭合。E2.1拖链系列具有坚固的限位块,能够增加25%的架空长度和100%的填充重量,同时自重比同类型拖链轻10%。链节限位块上的“制动器”能够确保拖链安静运行。因此,这一拖链系列在自动门、车辆和医疗家具等应用上具有出色表现。   电缆保护和易于装配的设计 轻巧且坚固的E2.1微型拖链系列适用于各种要求的应用场景。现在,igus进一步扩大了E2.1系列的型号,新增3个内高尺寸,分别是26、38和48毫米。拖链的内部轮廓光滑,能够有效保护电缆。与优化前的版本相比,新E2.1系列拖链在外高相同的情况下,内高增加了3毫米。针对拖链的内部设计,igus还提供圆滑的分隔片,以此延长软管和电缆的使用寿命。为了精准安装分隔片,横杆上注有刻度标记。 适用于狭小安装空间的chainflex高柔性电缆 为了让拖链和电缆达到最佳运行状态,igus研发出了拖链专用的chainflex高柔性电缆。例如,使用chainflex CFBUS.LB.060 Profinet高柔性电缆,能够在弯曲半径仅为7.5 xd的极狭小空间内传输数据。所有chainflex高柔性电缆均在占地面积为2750平方米的igus内部测试实验室内经过严格测试。所以,igus是全球唯一一家提供36个月质保承诺的电缆制造商。此外,为了方便客户更快速地开启应用,igus还提供即插即用的装配拖链,即由拖链和电缆组成的完整系统。


The terms "igus", "Apiro", "chainflex", "CFRIP", "conprotect", "CTD", "drylin", "dry-tech", "dryspin", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-skin", "e-spool", "flizz", "ibow", "igear", "iglidur", "igubal", "igutex", "kineKIT", "manus", "motion plastics", "pikchain", "readychain", "readycable", "ReBeL", "speedigus", "triflex", "robolink", "xirodur", and "xiros" are legally protected trademarks of the igus® GmbH/ Cologne in the Federal Republic of Germany and where applicable in some foreign countries.

igus® GmbH points out that it does not sell any products of the companies Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM,Parker, Bosch Rexroth, SEW, Siemens, Stöber and all other drive manufacturers mention on this website. The products offered by igus® are those of igus® GmbH