The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
IMM家具展上的新品:采用igus 3D打印弹簧的时尚葡萄酒柜22/03/2018
今年的IMM德国科隆国际家具展拥有11个展厅,占地面积达14.1万平方米,再次成为全球最大的家具盛会。在这里,家具行业的创意者们展示了各种设计和材料都独具匠心的新产品。 其中来自汉堡Gsechs应用科学大学的15位木工技术人员展示了由柚木/橡木、软木和石板制成的非常优雅的葡萄酒柜系列。而其中采用了免润滑且免维护的igus滑动轴承组件的旋转门设计更是独具匠心。 2018年IMM德国科隆国际家具展于1月15日至21日举行。众多公司和设计师在这里向全世界的观众展示了他们的新颖设计。来自汉堡Gsechs应用科学大学的15名学生也打造并展示了他们的作品——一个名为Dolio的葡萄酒柜系列,这个名字来源于拉丁语单词“dolium”(桶)。 这个系列的项目构思源自于一个以“不同凡响的打开方式”为主题的任务。在尝试了各种不同的原型之后,他们在数月内设计并制造出了20件的小系列家具。Dolio是一个立式的葡萄酒柜,可内置五瓶酒。一扇弧形的带有钢配件的石板饰面门可以绕着酒柜主体旋转360°,形成封闭空间。 为了确保旋转门能流畅地滑动,他们在钢配件上使用了极具耐磨性和低摩擦系数的iglidur B160耐磨带条。 此外,学生们决定自制锁门的弹簧。Jorrit Burmeister表示:“经过测试,我们决定采用igus的iglidur I150耐磨丝线来打印工程塑料弹簧夹。这种工程塑料坚固且适用性广,而且极具耐磨性,可以承受Dolio酒柜的持续载荷。” 易加工的免润滑耐磨部件 除了iglidur I150以外,运动塑料专家igus还有另外五款免润滑且免维护的iglidur耐磨丝线来满足不同行业的应用,例如需要永久负载或耐化学性的应用。这六款耐磨丝线的共同点是比3D打印标准材料高50倍的耐磨性。采用igus耐磨丝线进行3D打印是一个非常好的选择,尤其是复杂运动耐磨部件的小批量生产。igus还为没有3D打印机的客户提供3D打印服务,即采用iglidur耐磨丝线及专用于齿轮的激光烧结材料iglidur I3和iglidur I6制成客户所需的耐磨件。客户可以在线上传自己的应用参数,选择材料,计算价格和直接订购所需的耐磨件。 |