The selection of the country/region page can influence various factors such as price, shipping options and product availability.
Press |
|
Do you have any questions? Need material? Current press information and ready to publish photo material is available for download here. We would also be delighted about your call, e-mail or fax! |
|
Press contactWould you like to be added to our media distribution list? |
ロングストローク・横置き向けケーブル保護管 「プレーンチェーン」09/05/2019 インダストリー4.0で生産の自動化が進むなか、確実で省スペースなエネルギー供給ソリューションへの要求が高まっています。このような背景を考慮し、イグス株式会社(東京都墨田区)は、高速の長いストローク用に革新的な横置きサイド型のプレーンチェーンを開発しました。特別に設計された新型ガイドチャンネルに横置きのエナジーチェーンを装備することで、コンパクトかつフェイルセーフなエネルギーやデータの供給を実現します。 現在の生産現場を見れば、ロボット無しでは機能しないことは明白です。これは自動車産業において最も顕著で、リニアロボットやガントリー、あるいは産業用の7軸ロボット等、様々なロボットが活躍しています。これらのロボットには、限られたスペースや長いストロークで常に確実かつスピーディに動作することが求められるため、エネルギーやデータの確実な供給も必須です。自動化に向けてイグスが新しく開発したプレーンチェーンシステムは、高速・高頻度の用途で最大限のフェイルセーフを確保した運転を実現します。この新たなコンセプトでは、横置きサイド型のエナジーチェーンが特別なガイドチャンネルに配備されています。凸型形状のガイドチャンネルに設けた2本の窪みの中をE6型のエナジーチェーンが安全に走行し、摩擦係数が低いステンレス製ガイドチャンネルがエナジーチェーンの長寿命を確保します。また、設置高さが低く省スペースであることも利点です。ガイドチャンネル外側にオプションの特殊プラスチック製の防音層を装備すれば、システムの防音性を高めることが可能です。このエナジーチェーンは軽量部材を採用しているため、天井の下のリニアロボット用に容易に取り付けられます。 |