Change Language :
Additive manufacturing processes are part of digital production. Regardless of 3D printing method, each new component must first be designed as a digital 3D model, which can then be used for production without the need for further component-specific tools. This process offers numerous advantages:
In SLS 3D printing, plastic powder is applied in layers using a doctor blade and melted with a laser at the point where the component is to be created. This process is characterised above all by its cost-effectiveness, fast production and high dimensional accuracy of the printed components(from ± 0.15 mm).
Further advantages:
Tip: Compared to the SLS process, FDM 3D printing offers a greater variety of materials.
FDM is a 3D printing process in which a meltable material (plastic) is heated and applied layer by layer via one or more nozzles. This is also referred to as filament deposition or filament extrusion. The inexpensive purchase of a filament printer and the simple handling make FDM the most widely used 3D printing process.
Special services at igus®:
Tip: If support material is to be dispensed with and components with a high layer bonding and higher dimensional accuracy (< ±0.2 mm) are required, the SLS and DLP processes are better suited than FDM.
DLP is a 3D printing process in which layer after layer of synthetic resin is exposed to UV light in a tank and thereby cured or polymerised. A UV light source hits an array of mirrors, which reflect the light as a two-dimensional layer geometry and cast it onto the material.
Advantages:
DLP vs SLA:
A major advantage of 3D printing using the DLP process is the time saved. Compared to the SLA process, in which each point is individually exposed by a laser, the resin is cured surface by surface in the DLP process, thus reducing the construction time many times over. In addition, the resolution is significantly increased with up to 35 µm pixels.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h