Change Language :
Cleanroom chains also play to their strengths on long travels. Here, the upper run of the cleanroom-compatible E6.52 energy chain is supported over long travels, eliminating particle emissions from gliding. Motor-controlled rocking of the roller guide minimises contact. In the area of the travel through which the radius of the energy chain does not pass, it is possible to save costs with the new support with fixed roller as the rocker mechanism is not required there.


| Part No. Support plate | Part No. e-chain series | Inner width [mm] | Bend radius [mm] | Support gap [mm] |
|---|---|---|---|---|
| GLO.CR.56.R | E6.52 | 50 - 300 | 075 - 250 | 1,000 - 2,000 |

1. cleanroom-compatible roller supports
2. Contacts are minimised by motor-controlled roller guide rocking.
In addition to its long service life, the E6 system offers numerous other advantages. For example, it is characterised by extremely quiet, low-vibration operation - making it a good match for the low vibration drive concept of the linear motor. The so-called polygon effect, which can occur when an energy supply system is unrolled, is reduced to a minimum. The ultra-low noise levels have been confirmed in an expert report by TÜV Immissionsschutz und Energiesysteme GmbH.

Free white paper:
In this white paper, you will learn how you can use the right energy supply in the cleanroom to


Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h