Change Language :
A hybrid cable is known as one-cable technology. Their use makes it possible to save both money and time. Up to now, the servo motor and the converter have always been connected to two cables: A servo cable was used for the power supply.
For the data re-transmission, an encoder cable is provided to inform the control system, for example, the speed and position of the motor. Energy supply and data transmission run on a single cable, a so-called hybrid cable. This eliminates the need for cabling with a separate encoder cable for the encoder.

In our online shop, discover surplus cable lengths at a 50% discounted rate!
These set lengths from the standard range maintain the same quality as the rest of our chainflex® cables and are backed by a 4-year guarantee.
Simply visit your desired cable within our shop and check for surplus lengths available at half price.
A major manufacturer of woodworking machines converted its drive technology to the new Beckhoff hybrid technology, capitalising on the advantages of the more compact design. The challenge was with the cables, which in their machines have to perform a great many movements with very tight radii. This is where igus entered the race with a challenging service life test. It was challenging because the requirement was to also measure the Hiperface DSL bus data transmission over its use. That is why we worked very closely with our customer to achieve reliable results for both of us. Feel free to send us a query when you need to test cable solution durability.

Hybrid technology is the biggest trend in the cable industry in recent years and is also known as One Cable Connection (Siemens) or One Cable Technology (Beckhoff). With this technology, four power cores (L1, L2, L3 & PE), a pair e.g. for temperature monitoring and cores for a bus system are usually combined in one cable. Each major drive manufacturer uses its own bus system; Beckhoff, for example, uses the Hiperface DSL bus system from SICK, while Siemens uses an Ethernet derivative. We at igus have followed this technological trend and optimised the mechanical cable design for the energy chain. Our hybrid cables CF220.UL.H and CF280.UL.H can be easily connected to the drive systems of the major OEMs.
For more information on the topic of drive cables and their manufacturer's read what we have to say in the below blog.

A hybrid servo cable is a cable consisting of both a servo cable and an encoder cable. Hence the term “hybrid”. This type of cable tends to be lower cost and space efficient and with the “one-cable” technology this might be one of the reasons for the increased popularity. Consumers are a fan of the all-in-one product.
Until recently, the servo motor and the converter were connected to two cables, the servo cable for the power supply and an encoder cable for the data re-transmission. This combination provided information to the control system about varying elements of the power source such as; the speed and position of the motor.
With this increased popularity, more and more drive manufacturers have been offering servo motors with this one-cable solution. The ability to have an energy supply and data transmission running on a single cable eliminates the need for cabling with a separate encoder cable, it is all integrated.
As previously mentioned, each drive requires two cables – the motor cable and the encoder cable. By creating a hybrid servo cable, this combination in a single cable creates room in the energy chain and the motor connection area, as half of the components are not required. This cable arrangement can save space and money as it effectively allows the double cable to become a single one. Due to the combination of two cables, you not only save on material but also space and installation time. The hybrid cables are ideally used wherever servo motors are used.
A good example of the use of our hybrid servo cables is in machines working at high speed. By using the latest servo technology, high dynamics in combination with positional accuracy and fast feedback can be implemented.
We achieve good shielding effects by strong coverage of necessary elements and a flat braid angle that ensures that the properties are retained for a long service life, especially in moving applications.
With the igus® range of chainflex® cables being so vast, it is not surprising that we have various options when it comes to hybrid cables.
For the hybrid servo cables, we have examples such as the CF280.UL.H cable, ideal for the packaging industry and handling equipment applications. The wide operational temperature range means they can be used for both indoor and outdoor environments, which when combined with its almost unlimited oil resistance, opens many doors in terms of applications these cables can be used for.
We also have hybrid robot cables which can withstand torsional stress, are resistant to oil and are flame retardant.