Change Language :

In our online shop, discover surplus cable lengths at a 50% discounted rate!
These set lengths from the standard range maintain the same quality as the rest of our chainflex® cables and are backed by a 4-year guarantee.
Simply visit your desired cable within our shop and check for surplus lengths available at half price.
Shield and filling material
The structure of the robot cables is significantly different compared to the cables for linear applications. Normally, our cables have a very firm and strong internal structure to withstand the special conditions in linear chain applications. In a torsion application, however, there are completely different arrangements. These cables have a very soft structure to compensate for the torsional movements. The difference is particularly noticeable in the shield and the large number of fillers. We have a different shield concept for robot cables. Here we use a shield wrap and not a shield braiding, because with a winding the shield can adapt to the torsional movements and open and close. We have also integrated many fillers into the cable. These have the function of a shock absorber and cushion the torsional movement within the cable.

Robot application
For a robot that welds, clinches, screws or glues thousands of cars every day, things really get down to business. Not only does the cable need the capability to be twisted, it also has to be abrasion-resistant and bendable around small radii. It is a very demanding movement. We have done a lot of research here to make the cable with the chain a reliable system for the robot. In various tests with major automotive companies, in their applications and in specially developed cable testing machines, we gained experience that enabled us to further develop our product families for the most extreme applications. In the past, our customers had to have expensive special designs manufactured in large quantities. Today, however, they benefit from the resulting catalogue product range for robots.

Each robot manufacturer uses different core/cross-section combinations depending on the robot. These combinations are determined by the respective drive and measuring system of the robot.
For example, a FANUC robot must of course be supplied completely differently to a KUKA robot or one from ABB.
Even within the respective manufacturers, the robots use different cable constructions depending on their design.
In the CFSPECIAL.792 series, we have mapped the common designs. This enables customised use even for small quantities. As the robot is generally plugged in, we can supply the cable harnessed in the desired length. Simply tell us the robot type in question and we will offer you a ready-to-plug-in solution.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h