Change Language :
Several million work cycles per year with maximum precision in the micrometre range and five years of maintenance-free operation: Häcker Automation GmbH develops and manufactures machines for micro-assembly that meet the highest requirements. The Schwarzhausen-based company also leaves nothing to chance when it comes to partner companies and components. Today, cables and energy chains from igus® are used for the energy and data supply.
"The cables must be optimally guided in the chain - especially when the chain is tightly packed. The bend radius must be taken into account as well as the internal separation and effective strain relief. The cables must not show any movement in the chain, but they must not be fixed either: A lot of detailed engineering is required here, in which igus® provided us with excellent support."
Jens Beyer, technician at Häcker Automation GmbH
Designing the cable carrier
for the cable carrier system. Detailed work is also always required here, which igus® and Häcker did together. Jens Beyer: "The cables must be optimally guided in the chain - especially when the chain is tightly packed. The bend radius must be taken into account as well as the interior separation and effective strain relief. The cables must not show any movement in the chain, but they must not be fixed either: A lot of detailed engineering is required here, in which igus® provided us with excellent support." With success: Even energy chain systems with the smallest unwinding ranges of just 50 mm, which are used in the movement system for the dosing stroke, for example, achieve the extremely long service life required by Häcker. This is also remarkable because the cables and energy supply systems are subjected to high stresses due to the high speeds. But the design work that igus® has carried out for Häcker guarantees high availability over long periods of time. Convincing solutions were also developed for special requirements - for example, igus® was able to offer an energy chain-compatible PE cable with a 1.5 mm2 cross section for the energy chain system at Häcker following tests in the laboratory. The detailed
work includes the chain fastening, which is structurally integrated into the energy chain system, and the selection of the cable. The high demands on service life make it necessary that only tested components are installed. This applies to the energy chain as well as to the cables, which are supplied ready-made as readycable® from igus® : Then the assembly personnel in Schwarzhausen do not have to do the assembly work and can connect the complete cable set including plug connections directly. This saves time, and that is what counts at Häcker: only a throughput of ten days is estimated for the construction of a machine.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h