Change Language :
Direct drive technology is also becoming increasingly popular in machine tool construction. Non-productive times and set-up costs are being further reduced and machining speeds are increasing. After receiving appropriate advice on site, a long-established company has equipped its two-spindle horizontal machining centre with particularly quiet and low-vibration energy supply systems that easily meet the technical requirements for dynamics and acceleration.
Saalfelder Maschinenbau GmbH - a company with tradition
"We can look back on over 130 years of experience in machine tool construction," says Dipl.-Ing.-oec. Simone Stadermann, Assistant Sales Manager, about Samag's company history. At the Saalfeld site, the mechanical engineering division develops and builds two- to four-spindle horizontal machining centres for medium and large-scale production. In addition, there are special machines and multi-spindle deep-hole drilling machines. "We see ourselves as a solution provider. Whether light metal or heavy machining tasks - our systems flexibly and reliably handle all customer-specific requirements," says Simone Stadermann.
In the second business division, Automotive, parts are machined for medium and large series production. These are engine and drivetrain assemblies for the automotive industry. These include axle housings, lid, bevel gears, differential compensation housings for axle drives and engine crankshaft bearing covers. "We use our own machining centres for the complete machining of the workpieces. This means that our customers benefit from the synergy effects of machine tool construction and parts production. In addition, we can show our machines and systems in action at any time," explains Simone Stadermann. "From practice and for practice, they secure decisive competitive advantages!"

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h