With the "Compact plus", B. Braun launched a newly designed perfusor series on the market in 2017/18. The new development was necessary due to changes in international and national regulations, which have a major influence on the design and functions of medical devices. The new perfusors are equipped with numerous safety functions. Dr Dirk Aljets, Lead Engineer Infusion Pumps of the "Compact" series: "The device recognises the inserted syringe, for example, and monitors all essential processes itself. The control system is redundant; the two processors communicate with each other and report immediately if they detect deviating values." And only when the device has recognised the syringe is it locked and the drive started.
The operator guidance is designed with usability in mind: Many syringe types and active ingredients are stored in the integrated database. The operating theatre staff enter the delivery rate, which depends on the patient's weight, for example, and can rely on this value being precisely adhered to. Predefined infusion profiles are also possible. Dr Dirk Aljets: "With some active substances, a bolus, i.e. a certain level, must be reached quickly first, then only a subsequent dose is administered."