Change Language :
Motion Solutions GmbH's products - power wheelchairs and rehab therapy systems - are all about the mobility of the people who use them. The products themselves are also extremely mobile - for example, the active seating system for wheelchairs, which can be adjusted in various directions, or the heavy-duty wheelchair for people weighing up to 350 kilograms. When designing these devices, the designers utilise our lubrication-free bearing technology and compact energy supply.
A recent new development from Motion Solutions is an active seat module that can be installed in existing wheelchairs and provides an amazing amount of mobility: the user can recline the backrest and seat to an overhead position. They can also tilt the seat forwards by up to 33 degrees - in the opposite direction - to help them stand up. The entire seat can also be tilted 20 degrees to either side. As the movements can be superimposed, the user ultimately sits as if on a large ball, whereby the position is held securely in any position. This is by no means just a gimmick, but promotes the health of physically disabled people. A healthy person who is seated is constantly shifting position. This is often not possible for a power wheelchair user. The possible consequences are circulatory disorders or even open pressure sores. With the seat module, the user can shift their position and specifically promote circulation or simply transfer over the trade show stand. All angles of the seating system can be programmed to automatically and alternately relieve pressure on one side and then the other.
Here, too, the user's mobility is encouraged - with highly manoeuvrable drive systems. The scissors of the cardan system, which are protected by a bellows, are equipped with iglidur ® plain bearings. And the design engineers at Motion Solutions don't just use bearing technology from igus®: They use our plastic-energy chain for the energy supply to the movable, adjustable components of the power chairs.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h