Change Language :

Save costs on long travel distances with energy chain systems
Motorised cable reels or cable reels can be used as an energy supply for long travel distances - for example in the bulk goods or crane industry. They are relatively easy to install and generally do not require a guide trough to keep the cable on the desired path. igus®, a manufacturer of components made from high-performance polymers, offers complete energy chain systems as an alternative to motorised cable reels, which are particularly advantageous for long travel distances.

The advantages and disadvantages of both energy supply systems in industry
Whenever designers have to guide hoses and energy and data cables in moving applications with long travel distances of over 100 metres, the question arises: Which cable carrier system is the most efficient - in terms of reliability, ease of maintenance and future-proofing, among other things? A motorised cable reel? Or an energy chain? The advantages and disadvantages of both systems.
Energy chain systems have no slip ring, which is the reason it is also possible to transmit media such as air, water and oil without interruption.
Various cables and hoses for energy, data and media can be safely managed in one system and individually replaced or supplemented if necessary.
A motorised cable reel can run at a speed of approx. 300 m/min. For the first few metres, the pace must be reduced for safe rolling. For medium feed, this means that the system must be braked and accelerated halfway. With an energy chain system, travel speeds of up to 600m/min are an option, and this is possible fully without any restrictions on the loads or speeds at start-up.
Energy chain systems do not require their own drive, they are simply attached to the moving part of the system and carried along.
Depending on the travel/cable length, a motorised cable reel has a diameter of up to 8 metres. In addition, space is required for the motor and the slip ring body. In the case of an energy chain system, irrespective of the travel, only one moving arm is required on the crane - which is integrated in the installation space of the crane - and the installation space for the trough of the chain on the ground.
In medium feed, half the travel length plus 20 metres reserve must be calculated as the cable length for motorised cable drums. In energy chain systems, one also calculates with half the travel length, but with only two metres in addition, which are needed for the radius of the chain. At higher travelling speeds (over 60 m/min.), however, end-fixed is recommended for motorised cable reels. This increases the cable length to the total travel length plus 20 metres reserve.
For maximum service life with optimised design - P4HD.56R heavy-duty roller chain
The new heavy-duty roller chain fulfils all the requirements that apply to container cranes of the next generation and beyond.
Ever longer distances, higher dynamics, short load cycles, zero failures: That, in a nutshell, is what manufacturers of ship-to-shore container cranes demand for energy chain on crane bridges. The new P4HD.56R fulfils these requirements - with maximum cost-effectiveness.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h