Change Language :
The igus products are used in the IPAnema 3 parallel cable robot. The support structure of the IPAnema 3 consists of a metal frame structure, but a suitable building structure can also serve as a frame structure for the cable robot. There are also compact winch units with servo motors and eight synthetic fibre or steel cables. The cables are connected to the mobile platform of the cable robot. By changing the cable lengths using the cable winches, the platform can be moved in all six degrees of freedom in space.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h