80% less working time thanks to readychain

Pre-assembled energy chains save space and weight in this machine tool series.

Profile

  • What was needed: energy chain of type E4.1L, energy chain of type E4/light, both designed as pre-assembled readychain®, chainflex® cable
  • Requirements: As the machine takes up just seven square metres, the chains also had to fit into a small installation space. It also had to be assembled quickly.
  • Industry: Machine tool construction
  • Success for the customer: The pre-assembled chains save the customer 80% of the installation time. The first machine with the readychain® has been in operation 24 hours a day, six days a week for more than 18 months without any problems.
UGrind 800 grinding machine with control panel and connected e-chains and accessories for workpiece feeding.

Problem

Solution

At the heart of the UGrind 800 S (standard configuration) is the multifunctional head, which enables external, internal and face grinding, external, internal and face turning as well as measuring.

The igus® cable and energy chain are pre-assembled with connectors in the z-axis to ensure a reliable supply of energy and media to the multifunction head.

The x-axis also contains a ready-made energy chain from the E14 series. By using the readychains, DVS Universal Grinding GmbH was able to save 80 per cent of its working time.

Contact us

Contact details

Opening hours