How to adjust drylin® T linear rail clearance

Why is adjustment important?

drylin® t clearance adjustment
  • reduce play
  • reduce vibration
  • Clearance adjustment
  • improve positioning accuracy
  • prevent binding and stick-slip
  • running surface optimised
  • increase service life

What are the main reasons for adjustments?

Step by step instructions and images of how to make an adjustment of the drylin T carriages

Step 1-

Hands adjust an igus DryLin T linear guide carriage with a wrench and screwdriver.

Step 2-

Hand adjusts an igus drylin T linear guide carriage with an Allen key.

Step 3-

Hand positioning a DryLin T linear carriage on a rail.

Step 4-

  • If the clearance has been adjusted too tightly so that the guide carriage is jammed, it is not sufficient to simply reset the Allen screws.
  • After screwing them back in, also press the reset button on the side opposite the screws to release the sliding elements again. Use a pin of the following size for this:
  • 2.5 mm for TW-01-20 and TW-01-15
  • 3.0 mm for TW-01-25 and TW-01-30
drylin T linear guide carriage on a rail.

Frequently asked questions

  • over tightening
  • issues with the parallelism of rails ( when more than one rail is in use)
  • if the carriages require lubrication, then a lack of lubrication can cause this
  • if the carriage or rail is damaged.

Contact us

Contact details

Opening hours