Plastic vs. Metal Bearings: Which Should You Choose?

The comparison- Metal plain bearings vs. igus plain bearings

Metal composite bearing vs. igus plain bearing

What is a metal composite bearing?

  • A classic metal composite bearing essentially consists of a metal cover and a very thin layer of polytetrafluoroethylene (PTFE).
  • Typically, these types of bearing have a maximum wear zone of approx. 0.05 mm or approx. 0.002 inches.
  • During operation, the PTFE layer is worn out.
  • In extreme cases, it is completely worn away until metal runs on metal, resulting in shaft damages or "seizing up" of the bearing.

What is an iglidur® polymer plain bearing?

  • iglidur® plastic bearings are made of modern polymer compounds, which consist of base polymer, solid particles and so-called solid lubricants.
  • These help reduce the iglidur® plain bearing's coefficient of friction.
  • A transfer to the shaft is not absolutely necessary, but improves functionality.
  • With this homogeneous structure, theoretically the entire wall thickness is available as wear zone.

Sintered bearing vs. igus plain bearing

What is a Sintered bearing?

  • The oil is absorbed by the body of the porous sintered bearing and provides lubrication, especially at higher rotation speeds.
  • The oil film necessary to ensure that sintered bearings function effectively does not work in the case of slow and/or linear or pivoting movements.
  • In addition, the amount of oil available for the duration of the operation decreases.

How do iglidur® plain bearings compare to sintered bearings?

  • The homogeneous and consistent structure with solid lubricating and reinforcing materials but without oil saturation ensures that the solid lubricants incorporated in the material are always available irrespective of the kind of movement.
  • Very low coefficients of friction and wear over the entire life cycle of the product.

Needle bearings

What are Needle bearings?

  • Due to the line contact between needle rollers and raceways, needle bearings have, compared to the point contact of the ball bearings, a better load distribution at the contact point during rolling
  • Despite this, the line contact requires a high Hertzian pressure.
  • Therefore, like all rolling bearings, they are sensitive to vibrations and shocks. In addition, wear of the shafts can occur, which is why usually hardened shafts have to be used.
  • Needle bearings can only absorb radial forces.

How do needle bearings compare tp iglidur® plain bearings?

  • Due to the large load-bearing surface and the comparatively elastic properties of the plastic, iglidur® plain bearings are also suitable for heavy shocks and edge loads.
  • Reinforcing fibres provide an additional improvement of the mechanical properties. In combination with iglidur® plain bearings, "soft" shafts can be used in many applications.
  • Even with edge loads, the risk of shaft wear is significantly lower than with needle bearings.

Conclusion:

Customer examples-| igus plain bearings replace metal bearings

High temperature

High-temperature applications

Heavy duty

The soil tiller prepares the ground.

Dirt

Dirt applications

Chemical resistance

Chemical resistance applications

Underwater

Underwater applications

Frequently asked questions