Change Language :
NFPA 79 - the Electrical Standard for Industrial Machinery - is part of the American National Fire Protection Association. The standard contains guidelines for designing the electrical system of a machine and shows ways to ensure machine operator safety.

It used to be difficult for machine designers to comply with the NFPA standard when using cables for moving applications. Until 2012, the NFPA standard did not allow the use of AWM cable. After the revision in 2012, the use of certain AWM cables is permitted, many of which can be used for highly flexible applications. Together with the UL standard, NFPA 79 is considered an important basis for compliance with the technical specifications for the electrical equipment of machines in America. Before a machine can be put into operation in the USA, it is checked whether the individual parts that make up a machine have been assembled correctly in accordance with the NFPA 79 standard.
The NFPA 79 standard describes the requirements that AWM cables must fulfil. Some of the most important requirements are summarised below.

For our chainflex® cables, this means the following:
With over 900 chainflex® types of control, bus, servo, motor and measuring system cables, we offer a complete, NFPA-compliant programme. With compliance to the conditions of the NFPA 79 standard and built according to the AWM standard, our chainflex® cables can be used in industrial environments without any problems.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h