Correctly securing plain bearings to prevent bearing drift

Causes of bearing drift, and solutions for perfect function

Glowing light bulb as a symbol of ideas, energy and technology.

Why does a bearing drift?

High temperatures

Excessive surface pressure

Inaccurate manufacturing tolerances

Damaged plain bearing with clear damage and defect from rotation in the housing.
Excessive temperature - the plain bearing rotated in the housing bore instead of running against the more suitable shaft.

The consequences of bearings drifting

How to prevent the drifting of plain bearings

  • Ensure that the temperatures do not exceed the maximum recommended value for the plain bearing.
  • Check the surface pressure to which the plain bearing is exposed.
  • Ensure that the tolerances of the housing bore and shaft are correct. At least an h9 tolerance is recommended for the shafts. Their inner diameter is only set after they have been press-fit into the H7 housing bore. Further information is available here.
Table of plain bearings for axial retention by temperature for various igus materials.
Table of plain bearings for axial retention by temperature for various igus materials.

Locating spigot of plain bearings

Bearing with undercut

Snap-on solutions

Flanging

Screw connection


Anti-rotation feature of plain bearings

Practical solutions for anti-rotation feature

Fixing holes

Positive fit on the outer diameter

Reworking the housing bore

Contact us

Contact details

Opening hours