Change Language :
This is the world's largest laboratory for moving cables. With 5,500m² of test area and over 800 tests running simultaneously on 64 systems, we achieve more than 2 billion double strokes a year to provide you with the highest quality technology.
The igus business units chainflex and readycable develop cables that are sold by the metre with plug-in connectors for direct connection to electric drives. Electric drives create motion by converting electrical energy from the power grid or from a battery into mechanical energy. chainflex cables are therefore the means of transporting electrical energy, thereby setting machines such as machine tools, robots or handling machines in motion.

In the area of drive technology, we have a large selection of high-end cables in our product portfolio. Very small bend radii in the energy chain in connection with long travels or extreme temperatures often pose major challenges for cables. Numerous tests in our test laboratory allow us to provide cables for the most demanding applications and extreme conditions that are of the highest quality and boast long service life.

Hybrid technology has been a hot topic for several years. Machine designers obviously would like to have only one cable that carries both energy to the motor and movement data such as direction of rotation, speed, and acceleration back to the frequency inverter. In addition to saving installation space on the cable and connector, the customer also eliminates the cost of processing a second cable and of the additional material.
We take all these advantages into account in the CF220.UL.H (PVC jacket) and CF280.UL.H (PUR jacket) cable series. Here, the electrical wire/cross-section combination is constantly being expanded to be fully compatible with drives from various manufacturers, such as Beckhoff, SEW, and Siemens. We use the digit after the letter "H" in the part number to mark this affiliation to the manufacturer's requirement. The advantage for our customers is that, if the article number is identical from the "H" onwards, they can choose freely between PVC and PUR jackets without putting themselves at electrical risk. This can result in great savings.
The topic of drive cables is currently being considered in detail in our energy supply blog. There are especially many articles dealing with hybrid cables - Find out about the latest technical developments, directly from the producer!

chainflex service life calculator
Go to service life calculator
readycable online configuration
Go to the online configurator"chainflex ... at home in the world" – This applies to drive technology, too, of course
All our cables have many approvals that allow worldwide use.
We have compiled a great deal of information about the world of standards in a booklet that we would be happy to send you.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h