Change Language :
Plain bearings are mechanical components which are designed to support rotating, oscillating or sliding movement between two surfaces. These components are used as a way of reducing friction and wear and unlike ball bearings, plain bearings function through frictional contact between the shaft and bearing.
Plastic plain bearings are manufactured using specially developed materials, infused with solid lubricants. This ensures the bearings offer low-friction and wear-resistant without any need for external lubrication such as grease or oil. There are a wide range available in differing designs, such as sleeve bearings, flanged bearings and thrust washers. Thanks to the polymer material, they offer lightweight, corrosion-resistant and maintenance-free solutions for a wide range of applications and industries.

There is always debates over whether plastic bearings can withstand the same loads, impacts and conditions as their metal counterparts but with the technology available today and the materials that have been developed over the years, the rise of the plastic plain bearing over the metal equivalent is huge.
Learn about the different plastic bearings that are taking the challenge of changing the misconception that plastic means weak....

We have a wide range of standard materials that our plain bearings are manufactured in which allows us to be able to offer materials for specific requirements such as chemical resistance, food safety, high and low temperatures, as well as environmental elements like sea water and UV exposure.
A plain bearing is a component that support 3 types of movement, rotating, oscillating and sliding between two surfaces.
Plain bearings support rotating, oscillating, or sliding movement between two surfaces. They slide instead of using rolling elements found in ball bearings and protect surfaces from wear. Plastic plain bearings use materials infused with solid lubricants, providing low-friction and wear-resistant operation without grease or oil.
A sleeve bearing is a cylindrical bearing, a flange bearing is the same but it has a flange at one end, often referred to as a "top hat"
Plastic plain bearings are more common than people realise. They can be used in most applications where metal ones can. If you use the online tool, it will help identify if a plastic plain bearing can cope with your application.
Self-lubricating bearings are bearings that require no additional lubrication, no oil or grease. These self-lubricating bearings are composed of thermoplastics and fibre reinforcements which means they are self-impregnated with solid lubricants. This ensures that the bearings can run successfully without additional external lubrication. Without the need for environmentally damaging lubricants, this prevents downtime, saves money, and reduces the impact on the environment.
Metal plain bearings can be lubricated with oils, grease or other lubricants. These can be costly, messy and cause issues in regards to maintenance time to keep the bearings in working order. One of the advantages about igus® bearings, as with all igus® products, is that they are lubrication-free. The range of plain bearings are manufactured in technical high-performance plastic which ensures the optimum running performances, longest and measurable service life and lowest friction values, all without the use of additional lubrication.
Plain bearings are used in a large variety of applications and industries, many of which require a cost-effective solution whilst maintaining a long service life. igus® plain bearings offer both of these elements, along with being lubrication-free and maintenance free. All of these attributes combined ensure a clean, smooth running movement within machines and applications.
In more than 12,000 individuals tests a year on over 200 test rigs in the igus® test laboratory, all materials are thoroughly tested. The findings go into a unique knowledge database on the tribology of maintenance-free plastic plain bearings. This database enables us to select the ideal iglidur® plain bearing for our customers depending on the application and to calculate its anticipated service life.
Automotive, medical, aerospace, agricultural to name a few but there are hundreds of applications that you can easily spot igus plain bearings in.
Yes we can! We have a range of tools and manufacturing methods which can help if you are looking for a bespoke component. If you have a more complicated part or a project, we have a dedicated team to help you
To the design service pagePlain bearings can be made from a variety of materials depending on the application, including:
The material is chosen based on factors such as load, speed, temperature, wear resistance, and environmental conditions.
igus provide an extensive range of bearing materials to suit all applications.

Office hours
Monday to Friday from 8 am - 8 pm.
Live chat:
24h